Other Parts Discussed in Thread: RF430CL330H, TRF7970A
Hi team,
Here's the request from customer:
- He has a requirement for short distance communication, with a maximum distance of about 1CM. The two devices are equivalent and use the same chip.
- The chip needs to support low power consumption mode as it is a smaller device that needs to support 3 years of work.
- The communication speed requirement is not high which is only simple information exchange.
- The existing schemes of TMS37157 all communicate with card readers. Does this scheme support communication between TMS37157 and TMS37157, which requires the device to actively initiate communication.
- He has also looked for other similar solutions, such as NFC mode of RF430CL330H (frequency 13.56Mhz), but P2P mode cannot be implemented.
- Is there a solution that supports peer-to-peer mode that can be recommended and meets his requirements?
Can you help to check this case?
Thanks and Regards,
Nick