Other Parts Discussed in Thread: CC2533, REMOTI, TUSB3410
3581.RemoteTI_target_module_schematic_v1.0.pdf
Hello!
I am lost...despite many documents.
I am working on CC2533 RF4CE Basic Development Kit. I would like to put a light on/off for example.
I noticed CC2533EM can be programming by the RemoTI target board via CC Debugger and I can't modify the Interface connectors (for example, I wanted to put the UART_RX to 0 and it's not possible since TUSB3410 seems be once programmed).
Consequently, I can't modify UART or SPI..
Therefore, I have a doubt: how lighting a phial since the remote controller device via CC2533 (with its antenna)??? The RemoTI target board is required for it??
Here the schema of the RemoTI target board and of CC2533.
Hope being clear,
Thanks
Regards.
Flo.