nice to meet you
I am a consultant for a company in Japan.
thank you.
The company I am currently consulting for is:
TI's TMS3705DDRQ1 is used for short-distance data communication.
I'm currently having the following problem:
If you check the data received from the sending side with the CPU that received it from TMS3705DDRQ1
Data may be garbled.
There are also bit errors, and there are times when the data is misaligned, such as 8 bits.
I've been looking into various causes, but I still can't find the true cause.
Please let me ask the following questions.
1) TMS3705DDRQ1, such as reception data is garbled or bit-shifted
Are you having problems?
2) I don't know if this is the cause of the above problem of garbled received data,
The peak value (amplitude) at the end of the receiving antenna becomes very small depending on the timing.
phenomenon is occurring.
I've been investigating various things, but at least I can't see any change in amplitude on the sending side,
For some reason, there is a phenomenon that the amplitude becomes smaller on the receiving side.
Since the antenna end is directly connected to the data reception port of TMS3705DDRQ1,
If the input impedance at the data receive port of the TMS3705DDRQ1 is
It seems that the phenomenon that it is getting smaller due to factors is occurring.
Have you ever had such a problem before?
Also, if such a problem occurs, if you know the cause and countermeasure
Could you tell me?
In particular, does the power supply voltage of the TMS3705 change the peak value of the antenna? Is there any chance that the wave height will be particularly small?
In addition, please let me know if the antenna peak value will change due to interference waves.
Thank you very much.