Part Number: TMS37157
This IC supports only half-duplex mode of communication (ie HDX, not full-duplex FDX-A or FDX-B). Can TI please confirm that it conforms to ISO 11784/11785 standards for animal ID, in HDX mode (or can be configured to do so)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS37157
This IC supports only half-duplex mode of communication (ie HDX, not full-duplex FDX-A or FDX-B). Can TI please confirm that it conforms to ISO 11784/11785 standards for animal ID, in HDX mode (or can be configured to do so)?
Hello Eddie,
the TMS37157 is using a TI protocol and is compatible with Texas Instruments' DST ("Digital Signature Transponder") transponder. It does not conform to ISO 11784/11785 standards.
Best regards,
Andreas.
Hi Andreas,
Does TI have any 134.2kHz passive transponder for ISO 11784/11785 animal-ID standards, either FDX-B or HDX communications mode, with a microcontroller interface?
Hello Eddie,
I'm not aware of a TI passive 134.2kHz animal-ID transponder with a micro-controller interface.
Best regards,
Andreas.