I am wanting to implement a RFID system into a current project. I want to place RFID readers in seats of a vehicle and the tags on people. The Readers need a read range of 2-3' but not much further, so that if a tag is picked up on the reader it can be identified and assigned to that seat location. The readers also need to be as small as possible as space is limited. The reader system will communicate with a microcontroller so I need a serial data output. Does anyone have any suggestions?