This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RI-TRP-DR2B-40 Reading issue Q&A

Dear Sir, 

Please check below Issue

1. I entered data into RFID tag, checked reading, and shipped tag. By the way, I received a call that one of the RFID tags cannot be read.

The reading failure occurred during initial Auto Packaging (TCAPS01) Manual Reading after get back the RFID tags that cannot be read, and also The reading failure in the RFID Portable Kit too,

After several consecutive reading tries with Tag in close proximity, it suddenly started to read normally (less than 10 times) Since then, all Auto Packaging devices have read normally.

2. The ‘RI-TRP-DR2B-40’ we are using is a passive RFID type and this method uses RF signals as a power source without a separate power source (battery),

We presumed that this RFID Tag with an error is a faulty power system (Tag Discharge).

<The requests>

Q1

What is the cause of continuous reading errors as described above and normal reading after several repetitions?

Q2

Is there a case like this? If any, is there an environment/factor where this error can occur?

Q3

The specification for the read and write range of RI-TRP-DR2B-40 would be?