This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8530: Application Related Configuration

Part Number: CC8530

Hello,

We are planning to use CC8530 for the below use case, Here we have one base station and three remote units. Each remote unit will have a mic input and headphone output. The mic data from each of the remote units are  transmitted to the base-station and the base station mixes this audio data from the remote units and transmits the mixed audio to each of the remote devices. The communication interface between basestation and the remote units is a full duplex communication link. The block diagramatic representation is shown below.

Kindly let me know if this configuration will work with CC8530 devices and in which mode we need to use the CC8530 devices.

Do let us know if we need to use 3x CC8530 devices or 1x CC8530 device at the base station side to realize our end application. 

Expecting a quick update, thanks!

Warm Regards,

DJ