Hello community!
I developed a 868 MHz RF device based on reference design "868 MHz Monopole PCB Antenna" (Design Note DN024). I copied the design as close to the original as possible and expected it to be compatible with SmartRFCC1110-868 module from "CC1110DK-MINI-868" development kit.
Two my modules work together normally, but when I change one of them to SmartRFCC they don't work - sent packets are not received. I connect both modules (my and SmartRFCC) to SmartRFStudio and using Continuous TX on one side and Continuous RX on another I can see that max RSSI level presents on the receiving end when a carrier frequency on the transmitting end is ~100kHz higher (another RF parameters are identical on both ends). So it may be supposed that the reason is in different resonances of module's antennas. But a bandwidth of antennas is much wider than 100kHz, so different resonance frequencies can't be the reason. Am I right? Probably there is another reason. Could anybody help me in this situation.
Thanks in advance.
Alexey