This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF430FRL152H: using analog linear potentiometer

Part Number: RF430FRL152H
Other Parts Discussed in Thread: MSP430F5310

  I've searched the help forum here for several days and while I've found a lot of interesting information, unfortunately I haven't quite found the exact information that I'm looking for.  I'm trying to design an NFC device using a Spectra Symbol ThinPot...it's an analog rectilinear diaphragm-type potentiometer that's 150mm long with 10 ohms resistance.  Using a spring-biased wiper, the potentiometer functions as pressure is applied at different spots along its length, and returns a voltage of a higher or lower amount depending on the wiper's position along it's length.  I went through a massive project using an MSP430F5310 as the MCU and a rectification circuit for power, basically paring down the NFC WISP that's used to be a popular project with some.  But looking at the RF430FRL152H, THIS is closer to what I have been looking for all along.  The literature that I have read relative to the RF430FRL152H indicates that it's already set up to use resistance-based thermistors...well, I was thinking, my potentiometer is resistance-based as well.  Although the readings from a thermistor aren't as linear as from the potentiometer I'm using, they are being converted externally anyways.  I realize thermistors have a time constant delay...my potentiometer has a bit of switch bounce delay happening as well when the wiper moves.  But anyways, could the V+ side of the potentiometer connect to VDD2X, the minus side to SVSS and the wiper to one of the ADC inputs?  Would a reference resistor be needed, if so?  I realize this Sigma-Delta ADC is a different animal than in the MSP430F5310.  How many times can the SD14 break down just 0.9V?  I'm just curious as to what the chances are making this work before I begin ordering the EVM board for the RF430FRL15xH series.  

Many thanks, sorry for goofy question here

  • Hello Customer, thank you for your question and interest in our products.

    The forum support of this product has been reduced to first reference our existing documentation and collateral. For support, please take a look to the “Similar Topics” section at the lower right of the thread page. In addition, please consult the existing collateral in the “Technical Documentation” section of the RF430FRL152H product web page along with the Frequently Asked Question document. Alternatively, you can use the search engine of your choice to look for related E2E threads. With each of these resources we believe it will help with your question.