Hello All,
In user guide of CC2530 it is mentioned in Timer2 section that "The timer can be started and stopped synchronously with the 32-kHz clock rising edge. Note that this event is derived from a 32-kHz clock signal, but is synchronous with the 32-MHz system clock and thus has a period approximately equal to that of the 32-kHz clock period."
Does that mean Timer 2 of CC2530 is using 32kHz crystal as a clock? If not, is there any other way to use 32kHz crystal with any of the timer module of CC2530
Can anyone update on this?
Harshal