This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sensitivity testing of CC1120 using '1010' pattern

Guru**** 317180 points


The best way to measure sensitivity is to use a signal generator that generates a package. For those with a mid range signal generator without the ability to generate a package an option is to use a generator to generate a '1010' pattern.

To set up a simple sensitivity test receiving a continous 1010 bit pattern do the following:

There are two ways to do this:

- Use the package RX feature in SmartRF Studio to show the bit error rate.

- Output the data on a GPIO pin for external processing

----------------------------------------------------------------------------------

Using Studio:

- Go to the package RX tab

-Set the SYNC word to 0xAA (SYNC3=SYNC2=SYNC1=SYNC0=0xAA)

-Turn of CRC:

PKT_CFG1_CRC.crc_cfg=0x0

- Set fixed package length

PKT_CFG0.length_config=0x0

- Set the package length to something that fits inside the Studio window or the length of the package used in the system, example:

PKT_LEN=0x10

If you have set the expected package count to 100 you will get the package error rate directly.

---------------------------------------------------------------------------

If you want the data stream out on a pin:

- Turn of preamble: set the package count

PREAMBLE_CFG1.num_preamble=0x0

- Set serial modus:

SERIAL_STATUS.ioc_sync_pins_en=0x1

PKT_CFG2.pkt_format=0x01

MDMCFG1.fifo_en=0x0

MDMCFG0.transparent_mode_en=0x0

Set the SYNC word to 0xAA (SYNC3=SYNC2=SYNC1=SYNC0=0xAA)

Turn of CRC:

PKT_CFG1_CRC.crc_cfg=0x0

Then set one IO pin to output the serie clock (IOCFGx=0x08) and one IO to output the serial data (IOCFG=0x09).   

The GPIO3 pin is found on pin 3 on P7 on TRX EB

The GPIO2 pin is found on pin 4 on P7 on TRX EB

The GPIO0 pin is found on pin 7 on P7 on TRX EB

The signal generator has to be set up to send a 1010 bit pattern and the frequency, bitrate and deviation has to correspond with whatever you have set up the chip to.