Hello everybody.
I have some problems with a frequency of the output signal of my board. It is (down) shifted by about 130 kHz compared to the nominal IEEE802.15.4 2.4GHz frequency grid. I've tried to cancel the offset with the help of FREQTUNE register but it allows only to decrease the frequency. Can anobody say if it is possible to solve the problem with increasing the capacity of external capacitors loading the 32 MHz crystal? or maybe another solution exists?
Regards,
Ilya