This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PER test not working on SmartRF04EB board

Other Parts Discussed in Thread: CC1101, CC1100

Hi,

 

I am trying to perform PER test on two SmartRF04EB boards with 2 CC1100/CC1101 EMK boards mounted on them.

The modules work in 868-915 Mhz range. I have done the below settings .

1) Press S1 for PER

2) Selected FREQ BAND as 868Mhz

3) Selected SET ID as 1

4) Selected PACKET LENGTH as 32

5) Selected # OF PACKETS as 131072

6) Selected PRESET 868Mhz as 2

7) Selected SELECT MODE as MASTER

8) Selected START PER

For the other SmartRF04EB board, I had done the same settings as above but with SELECT MODE as SLAVE

I am getting "Waiting for CONFIG DATA" in the slave board and LED2 glowing in the MASTER board.

I also tried burning the old firmware provided in the forum[0031] as a solution, but am still getting the same above response.

 

Please advise. Thanks in advance.

 

Best Regards,

NVS Shastri