Hello
I have a MSP-FET430UIF debugger device with a full installation (not Kickstart) of IAR Embedded Workbench, along with a CC430 board (EM-CC430F5137-900) and would like to test my C application on the CC430.
There are "READ ME FIRST" directions (as well as this PDF http://www.ti.com/ww/cn/uprogram/share/pdfs/MSP-FET430_flash_emulation_tool_user_guide.pdf) that came with the FET430UIF, and at section 1.4, step 3), my IAR workspace only has msp430x1xx through msp430x6xx targets available. There is no reference to CC430 or FETxxx_1.
Is there a way to program the CC430 using this debugger kit?
Thanks