This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 doesn't transmit moudulated output at SmartRF Studio7 v1.6.1.

Other Parts Discussed in Thread: CC2540, CC-DEBUGGER

I had operated CC2540 that was connected to CC-debugger and PC.

Until yesterday, version of SmartRF Stdio7 which I used is v1.3.2.

At "Continuous TX" mode of v1.3.2, frequency = 2440MHz, Tx Power = 0 dBm, and check "modulated", Spectrum analyzer shows modulated wave form.

At "Continuous TX" mode of v1.6.1, frequency = 2440MHz, Tx Power = 0 dBm,Spectrum analyzer shows below  wave form.

Unmodulated: 2439.999 MHz CW

Modulated: 2439.745 MHz CW

I think that modulated pattern is PN9.

Why is not a modulated wave pattern measured?

Next question, at "Packet TX" mode, is the setting value of packet interval is effective ?