Hi,
I have done a design with the CC1110 and a monopole antenna, like the "CC1110 minidevelopment kit reference board" and like DN024 design note, working in 868Mhz. The wide of my board is 63,5, it is wider than the monopole antenna (the wide of CC1110 minidevelopment kit is 40 mm). Thus, the ground plane in the base of the antenna is wider (63,5 mm), and there is pcb dielectric in both sides of the antenna. There are not any component in both sides of the antenna.
The DN024 specifies a length of 20 mm for the last segment of the antenna (L4 in DN024) with 868 MHz. With the new board, must the length be longer o shorter than 20 mm ?. How can i tuned the antenna?
regards,
José R. Quintanilla