I'm in the process of getting my scripts ready for certification testing of my CC8520 design. I know I have to create a special hex file with the EHIF commands using the GenAutoProdTestImage.exe program. What I'm wondering is anyone has already created the EHIF command scripts or can direct me to an app note that describes what set up I'll need. From what I understand, I'll need to provide three separate setups, one to transmit using the upper channel, one to transmit using the middle channel and one to transmit using the lower channel. I believe I can do this using the RFT_TXPER EHIF command by setting the RF_CHANNEL field to 18, 9 and 1, respectively. I'd like to confirm this before testing. Thanx!