This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A working with RI-TRP-R9QL

Other Parts Discussed in Thread: RI-TRP-R9QL

Hi All,

I will be getting the TRF7970AEVM. I would like to know if this will work with RI-TRP-R9QL?
Do I need to write anything to the transponders to get it running?

Regards,
Poh Leong

  • Poh Leong,

    please note that the 2 items are not compatible: The TRF7970 is an HF 13.56MHz system, the RI-TRP-R9QL-30 is an LF HDX part working with LF Readers 134.2 kHz only. The RI-INL-R9QM-30 would wok with the eval kit RI-K3A-001A-00, the TRF7970 kit supports HF tags ISO15693 such as the RI-I03-112A-03 and also NFC compatible devies.

    Best regards,

    Klemens