This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P7: About Spurious emissions

Part Number: CC2652P7


Tool/software:

Hello,

 

My customer is asking Spurious emissions on CC2652P7 datasheet.

According to spurious emissions(datasheet page 18), note(1) is described below.

(1) To ensure margins for passing FCC band edge requirements at 2483.5 MHz, a lower than maximum output-power setting or less than

100% duty cycle may be used when operating at 2480 MHz.

 

About " less than 100% duty cycle", what does this duty cycle mean?

 

Regards,

Tao_2199