This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
CC2652RSIP module what I understand is there is a PCB Internal Antenna of 2.4 Ghz inverted F Antenna with maxinum gain of +3.3 dbi
when I try to transmit RF data packet from Smart RF I can use this internal Antenna itself.
my question is
question 1 : whether CC265RSIP has external antenna? Give me a details
question 2: how to disable the internal antenna
question 3: how to use external antenna
question 4: how Internnal antenna works I need to know the effect of radiation from the internal antenna
Question 5 : how to connect CC-Antenna-DK2 with CC 2652RSIP
Hi Kumaravel,
1. The CC2651RSIP does not use an internal antenna. See the image below:
2. No internal antenna to disable. Internal antenna is only supported in MODA or SIPA package.
3. Populate the matching circuit shown in the schematic.
4. Internal antenna is only supported in the MODA or SIPA packaging, but if you need it I will search our repository for it.
5. Have configuring the board to conducted, U.FL connector and using an RF cable.
Bun
I am using CC2652RSIP which has internal antenna right?
how it works to send data via RF drivers when internal antenna is not present
my question is CC2652RSIP I am not connected with any external antenna and there is no internal antenna also but when I send data from the smart Rf or CCS my packet data is been transfered .
How it internally works
What I understand is data in thr RF core is been transmitted due to lickage of radiation via external antenna Is is right?
TX transmission with the internal antenna should not be possible with the RSIP package as none exist. Are you sure you don't have the RSIPA?
Bun
I have noticed that their is an integrated pcb antenna within the launchpad
I am also attaching the inverted antenna datasheet for your reference
My query is how to connect external CC-Antenna-DK2 kit
can you please help me by giving the full setup as an example of connecting the external antenna
See section 2.1 of the Antenna Summary: https://www.ti.com/lit/an/swra496a/swra496a.pdf