Part Number: CC2340R5
Tool/software:
I would like to develop a product using the CC2340R22, which is a chip with 256k flash and 32k RAM. I am currently developing with the latest SDK version (8.10.01.02). I noticed that there are no folders related to the CC2340R22 in the `source\ti\devices` and `source\ti\boards` directories. Additionally, I've found that the flash size for the CC2340R5 is different from the R22, and the RAM size for the R2 is different from the R22. I am unable to locate the appropriate files for the CC2340R22 within the SDK. Please advise me on how to proceed with development using this SDK.