Tool/software:
Based on the standard circuit published by TI, I created a wireless circuit using the CC2543RHBR and XRCGB32M000F2P10R0 (Murata).
When I checked with a spectrum analyzer, I found that as the ambient temperature rises, the wireless frequency starts to shift.
This phenomenon occurs when the temperature rises by approximately 122°F from the start of operation. For example, starting at 68°F, the wireless frequency starts to shift around 158°F, and at around 176°F, the frequency drifts by more than 10 MHz.
Resetting the power to the wireless circuit restores the wireless frequency to normal.
This phenomenon also occurs when the temperature decreases. (For instance, after resetting the power at 167°F, the phenomenon occurs as the temperature drops to around 77°F.)
Does anyone know the cause of this issue or have any potential solutions?