Hi,
We want to develop hardware for wireless electronic musical instrument interfaces.
None of the existing protocols (like BLE, Zigbee, Thread etc) meet our requirements. So we want to make a custom protocol.
But it is beyond our reach to do a full RF certification for CE and FCC.
If we understand correctly it is possible to use pre-certified modules and build on top of one of the base protocols these modules are certified for. This way you can do a more simple CE and FCC certification test.
Which (certified) protocols can we use to build our custom protocol?
We would like a transfer rate higher then 250Kb/s. more like 1Mb/s or 2Mb/s. Is that possible for custom protocols?
Can we for instance use the lower layers of BLE for this (without the need of module re-certification)?
Can we use the SimpliciTI SDK to build our high speed protocol without the need for module re-certification of CE and FCC?
What exactly are our options?