Part Number: CC2652PSIP
Tool/software:
Hi,
I am attempting to use a gp timer in edge capture mode so I can count digital pulses. Is there an example that I can reference to do this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2652PSIP
Tool/software:
Hi,
I am attempting to use a gp timer in edge capture mode so I can count digital pulses. Is there an example that I can reference to do this?
Hello Chris,
We may not have an exact example here, but we can try modifying the period example to use edge capture:
(reference the SDK documentation by pressing the "GPTimer Driver" hyperlink)
GPTimerCC26XX_Handle hTimer;
void timerCallback(GPTimerCC26XX_Handle handle, GPTimerCC26XX_IntMask interruptMask) {
// interrupt callback code goes here. Minimize processing in interrupt.
}
void taskFxn(uintptr_t a0, uintptr_t a1) {
GPTimerCC26XX_Params params;
GPTimerCC26XX_Params_init(¶ms);
params.width = GPT_CONFIG_16BIT;
params.mode = GPT_MODE_PERIODIC;
params.direction = GPTimerCC26XX_DIRECTION_UP;
params.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
hTimer = GPTimerCC26XX_open(CC2650_GPTIMER0A, ¶ms);
if(hTimer == NULL) {
Log_error0("Failed to open GPTimer");
Task_exit();
}
Types_FreqHz freq;
BIOS_getCpuFreq(&freq);
GPTimerCC26XX_Value loadVal = freq.lo / 1000 - 1; //47999
GPTimerCC26XX_setLoadValue(hTimer, loadVal);
GPTimerCC26XX_registerInterrupt(hTimer, timerCallback, GPT_INT_TIMEOUT);
GPTimerCC26XX_start(hTimer);
while(1) {
Task_sleep(BIOS_WAIT_FOREVER);
}
}
Thanks,
Alex F