Tool/software:
Dear Specialists,
My customer is considering TRF7964A and has a question.
I would be grateful if you could advise.
---
The TRF7964A has two inputs, RX_IN1 (pin 8) and RX_IN2 (pin 9).
Is it correct to understand that data sheet 6.4.1 states,
"Monitor the RSSI of each of the two inputs and select the better one using bit 3 of chip status control register 0x00"?
If only the main input is used, is it possible to use RSSI of the auxiliary input is 0?
---
I appreciate your great help in advance.
Best regards,
Shinichi