Hi,
At our lab we have two different batch of PCBs of same design, ordered at different time, from the same vendor, (say Batch-1 and Batch-2), and my observation as follows,
1. The Packet Tx & Rx communication works fine between the Batch-1 boards and no change in the Smart RF tool is required.
2. The Packet Tx & Rx communication works fine between the Batch-2 boards and no change in the Smart RF tool is required.
3. When the Packet Tx & Rx communication tested between Batch-1 board and Batch-2 board, there was no packet transfer. When the Rx Filter Bandwidth at the receiver side is increased (for 2.4kBaud, the Rx BW increased to 222kHz), then the Packet transfer works fine.
So, my query is, How to over come this situation, and establish the Packet transfer between different batch of boards?
Please clarify.
Regards,
Kamesh Kumar S