Tool/software:
Hi All,
We are considering the CSTCR4M00G55B-R0 as a clock source for the TMS3705FDRQ1.
We are trying to check whether the frequency deviation of the ‘CSTCR4M00G55B-R0’ is a problem for the ‘TMS3705FDRQ1’ for adoption.
However, the fosc frequency is only listed as 4 MHz (NOM).
Therefore, please tell me the MIN and MAX.
Best Regards,
Ito
Ito,
The allowable frequency deviation of the TMS3705-Q1 device will depend on the receiving device it will communicate with. Typically the receiving device will have a min and max allowable frequency it can receive. This will dictate the 4MHz variation allowed on the TMS3705-Q1 device side for proper operation.
The resulting output frequency of the TMS3705-Q1 can be calculated by taking the measured 4MHz clock input, multiply it by 2, and then divide it by 119 to get the resulting LF frequency.
Regards,
Andrew