This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What do I need to use the Packet Sniffer?

Other Parts Discussed in Thread: CC-DEBUGGER

Hello,

I want to use the SmartRF Packet Sniffer on a 868MHz frequency. At the moment I am confused which hardware I need for this job. The CC1111 Dongle appeared to be the right tool for the job. From what I read on the forum I get the impression, that I only need a CC Debugger to flash the Dongle, change the register settings and use the Packet Sniffer, but in the CC1111 Dongle description it is written, that a CC1110DK is needed for this operations.

When I searched for a CC1110DK I found the Mini Development Kit and wondered if it is compatible with the Packet Sniffer and is the one thing I need and nothing else.

Could you please help to clear up my confusion?

  regards,
Martin