Hi all, From the CC2520 specification, it says it provides 'packet sniffing mode.' It seems it provides a packet sniffing function for a predefined channel. However, I'm interested in implementing a CC2520 based 802.15.4 packet sniffer which can simultaneously scan all the 16 channels. Is it possible to implement such a packet sniffer which can simultaneously scan all the 802.15.4 channels without channel hopping? If not, could you provide me with any possible idea? Thank you.