Part Number: CC2650
Tool/software:
I am attempting to connect a DS1820 sensor to the Lanchpad CC2650 board using DIO7 as the DQ line. When I power on the board, I set DIO7 to input mode, but I cannot read any high level. My power output is from the board's built-in 3.3V power port. I would like to know what issue may have arisen with my GPIO port configuration (the circuit setup should be fine, as I have tested it using other methods)