TRF7963A: Timing Conditions for MOSI With Respect to S_CLK

Part Number: TRF7963A


Hi

Question regarding issue mentioned in: Application Report SLOA1408B, section 1.7: Timing Conditions for MOSI With Respect to S_CLK


I am using TRF7963A in SPI mode with SS

  1. Is this issue relevant for TRF7963A?

  2. Is this issue only relevant when SS active (TRF7963A)?
    Or is it also relevant when communicating with other devices on SPI bus (when SS high)?

  3. How to recover?
    In case of ‘failure’, does TRF7963A switch back to SPI mode on next SPI chip select (SS high, SS low again)?

Regards Knud