I wonder why PA_TABLE settings for various frequency bands are not monotonic functions of output powers? For example, for 868 MHz, -10dBm is 0x27, -5dBm is 0x8F while 0dBm is 0x50. And it also weird that the maximum power setting is 0xC2 instead of 0xFF. Can anyone shed some light on why PA_TABLE setting is designed in this way? Thanks!