I am designing a peer-to-peer system using NFC devices, such as TRF7970a, for Industrial Control. The concept is to have a NFC target mounted on the end point that can communicate with a hand held controller. The target will not have its battery but will be powered on by the RF field of the controller when the controller is in the vicinity of the target. I have the following questions about the design:
1. How do I power the TRF7970a and the MCU(MSP430) from the RF field?
2. How can I achieve a range of about 1mtr to 2 mtrs between the two RF7970a devices.
Thanks for the help.
Regards.
Hemant