Hello fellows.
I own a CC2430, and I copied the reference design of TI for this into my PCB.
The only difference is that my PCB's width is 1.6mm instead of 1.2mm (it does have 2 layers only).
I'm using a single ended antenna, which is connected in the red circle.
http://img41.imageshack.us/img41/6765/antennam.jpg
My questions are:
1. What should be the length of the antenna?
2. What should be the material the antenna is made from?
3. Should the antenna be bended (how if so) or should it be straight upwards?
I thank you very much for any help.
Shahar.