Other Parts Discussed in Thread: CC2530EM
Hi all,
I am using CC2530DK and I am trying to recreate the CC2530EM.
I tried using the gerber of the EM but it is just too small for me to create manually. I still can't have it fabricated. I still need to do some tests.
So what I did was modify the layout of the EM a little. Just enough for me to create it on my own. I separated the tracks and increased the diameter of the vias. Though I was careful not to touch the RFports and the crystal.
When I tried it out, I got a very significant decrease in RF power. Range was dismal and so was directivity.
With the EM, i could get a 1% PER for about 30m. But with my own module, range was a dismal 3m.
The tracks that I changed were those only on the GPIOs.
Here are pictures of the original and modified layout.
But here's the thing, not only is the layout modified, I am not sure about the dielectric I am using. Yes, it is fr4 - same as the EM - but I just learned recently that not all fr4s are made equal. Its characteristics are dependent on the manufacturer. For one thing, my fr4 thickness is 1.6mm, and the EM is 0.8mm. I am still waiting to here from our supplier about the characteristics of the fr4.
Does anyone know the characteristics of the EM's fr4.