We want to use the CC2591 with a CC2420 (not ready to switch over to the CC2520). The Reference designs on the website are based on the CC2520 and the CC2430 mated with the CC2591. Can I base a CC2420/CC2591 hardware design on the CC2520/CC2591 Reference Design, or is the RF output stage of the CC2420 different from the CC2520 (connect the CC2420 TXRX_SWITCH signal to CC2591 RXTX, but does it need to go to CC2420 balun)? If different, can you provide the necessary information to use the CC2420 with the CC2591?