Hello,
I plan to use the CC1101 chip with the 0896BM15A0001 matched BALUN from Johanson Technology (see DN025) and the 0868AT43A0020 chip antenna from Johanson Technology (see DN016). My question: what should the matching network between the matched BALUN and the chip antenna look like? Is it OK to use the network as shown on page 4 of DN016 (12nH and 1.8nH) or should I use a combination of the network on page 4 of DN016 (12nH and 1.8nH) and page 4 of DN025 (L122 and C123) or maybe even an other network.
Thanks in advance for your help/suggestions.