Other Parts Discussed in Thread: CC2430
The document swra168a mentions that CC11xx PCBs should have 0.8-1.0mm (~31-39mil) distance between the top layer (containing the RF section) and the 2nd layer (solid ground plane). The reference design for CC111x indicates that a 1.6mm (~62mil) thick FR-4 PCB should be used, however the PCB layer stack-up thicknesses are not mentioned (nor are any specific dielectric constants).
Since PCBs should be symmetrical, the distance between layers 3 and 4 should be the same as between layers 1 and 2, which is 0.8-1.0mm. However, with two 0.8mm cores and a prepreg layer, the total thickness exceeds the target 1.6mm.
The nearest component reference design with layer stack-up info is the reference design for CC2430. It indicates that the distance between layers 1 and 2 (and between 3 and 4) should be 0.35mm, which is a lot more reasonable for a final PCB thickness of 1.6mm.
Can anyone clarify the situation? Is it because swra168a uses 2-layer boards?
What are the ideal PCB layer stack-up thicknesses for the CC1111 915MHz reference design on a 1.6mm-thick 4-layer board?
Thank you,
Alex