Ti has designed a PCB folded dipole antenna for CC25xx (Design Note 004).
I wan to know:
1) if this antenna could be used with CC2520.
2) if yes, the RF_P/RF_N on CC2520 has different space (1mm, there is a NC pin between RF_P/RF_N) than that of CC2500 (0.5mm),what is the best way to modified the original design to fit the antenna with CC2520 ?
3) if yes, what is the suggested way to deal with the NC pin between RF_P/RF_N? connecting to PWR? GND? or just floating?
Any advice would be highly appreciated.
BTW: I love this design because it requirs no balun device, which is very difficult for us to control the device quality and stability in tough environment.
UGlee