Other Parts Discussed in Thread: CC2430
Can someone from TI clarify if there is an error in Table 18 for pin 15 and 16 on page 18 in
http://focus.ti.com/lit/ds/symlink/cc2480a1.pdf
? It contradicts what I can see on page 20 here (and also in section "13.14.1.3 UART Hardware Flow Control" for the cc2430):
http://focus.ti.com/en/download/mcu/Accelerate-your-Zigbee-design.pdf
The definition of input and output are reversed. Sorry if I am completely off here...
So what I would like to have clarified once and for all:-):
1) Is RTS an input or output?
1a) How are the high and low level of RTS defined to do?
2) Is CTS an input or output?
2a) how are the high and low level of CTS defined to do?
3) Can you (please, please..) provide some sample code for the UART? Something where your sample files like "rpc_spi_cc2480.h" and "cc2480_rpc_spi.c" are rewritten to address the UART as well.
----------------------------------------------------------------------------
PS: I tried to ask politely:-) here:
https://community.ti.com/forums/t/2090.aspx