Other Parts Discussed in Thread: CC2520
hi,
I found a very small nice 32MHz crystal with 8pF load capacitance and I want to use it for my new CC2520 design.
Then I got an idea maybe this crystal may not need two external load capacitors anymore, because according to datasheet of CC2520, load capacitance = tune capacitance + parasitic capacitance + external loading capacitance, then if we assume 2pF as parasitic capacitance and 6pF as tune capacitance, then external capacitors are not needed anymore.
Is this way ok?
I know that 8pF means this crystal has higher sensitivity on environmental change, but it's 2*1.6mm small.