Hello,
I would like to know the actual frequencies that I should expect when the CC2520 is in CW test mode.
Can I assume they are the same as the channel frequencies? 2,405,000Hz, 2,410,000Hz and so on?
Thanks,
Lior
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to know the actual frequencies that I should expect when the CC2520 is in CW test mode.
Can I assume they are the same as the channel frequencies? 2,405,000Hz, 2,410,000Hz and so on?
Thanks,
Lior
Hi
When configuring CC2520, into CW mode using settings from SmartRF studio you get the frequency selected. Basically the centre frequencies of al 2.4GHz IEEE 802.15.4 channels are selectable.
Tor-Inge