This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 with PCB Antenna

Other Parts Discussed in Thread: 4428, CC2430, CC2530

I want to use  CC2530 + JTI balun ref design

4428.swrr065.zip

and replace the SMA antenna with a PCB Antenna

5824.swru120b PCB Antenna.pdf.

 

Should I follow the CC2430DB Reference Design 

8780.swrr034c.zip


to add a shunt and series component  same as CC2430 DB design at the feed point of the antenna, where L341 = L_1N8_0402_S and C341 = C_5P6_0402_NP0_J_50? 

 

Will a PCB Antenna works on a 2-layers PCB without  a Ground Plan?  Please advise. 

Thanks.

  • Wonderland,

    Yes you can use the CC2530 + JTI Balun ref design and replace the SMA antenna with the inverted F antenna. Please follow both designs as closely as possible. This will ensure the best possible results. Please use a series and shunt component at the PCB antenna feed point in order to tune the mismatch that may occur.

    It is recommended that you use a 4 layer board with a dedicated solid ground layer right under the component layer (top layer). A solid ground plane ensures shortest return paths for the RF signals, which reduces spurious emissions and allows you to pass specifications. So, it is critical to have ground plane.

    However, there should not be any ground plane under the antenna. There should be a copper exclusion layer that does not allow any ground around the PCB antenna.

    Again, please follow the reference designs as closely as possible.

  • Chatto,

    Please guide me how to pick the series and shunt component at the PCB antenna feed point for tuning the mismatch? Any application notes to discuss this? 

    Now the CC2530 + JTI Balun ref design has only 2-layers with ground traces.  Since you recommended a 4-layer board, my questions are:

    1)     Should I keep the top and bottom layers the same and just add a GND layer under the top layer? 

    2)     Also what will be the third layer, VDD or signals? 

    3)     Should I keep all the ground traces?

    Please advise.  Thanks.

  • Hi Wonderland,

    To tune the antenna you need a network analyzer. You solder a semi rigid coaxial cable to the feed point of the antenna matcing components (you have to remove the balun so the chip is disconnected) and you measure the impedance of the antenna. By using the smith chart you can calculate values for your matching components.

    You can stick to 2 layers and simply copy the CC2530+JTI reference design, but a 4 layer design will often have better performance. If you go for 4 layers, the second layer would be ground and the third can be used for a VDD plane and also some signal routing. You should fill all empty space on both the top and bottom layer with ground as well.

    /Fredrik

  • Thanks Fredrik,

    I have 2 more questions:

    1)     Will the matching components be difference for each PCB we build?  Or once we find the matching sets, we will be using the same sets for all PCBs we build?

    2)     Should I use the same matching set as CC2430 DB design at the feed point of the antenna, where L341 = L_1N8_0402_S and
    C341 = C_5P6_0402_NP0_J_50 as a starting point?

    Thanks again.

  • Hi Wonderland,

    1) The matching components will be the same for all equal PCBs. If you make a different design, with different ground plane size and shape you will have to redo the matching.

    2) Start off with 0 ohm resistor for the series component and do not mount the shunt component.

    /Fredrik