Hello all
I have buy some OEM CC1101 Chinese module on eBay and try to use it on my own devlopment board.
the SPI side is working fine. i can access to all registers.
i try to put one board in TX mode and send 10 bytes in loop, each seconds. and would like to receive it on the other board !
i request help because it's not working !i don't know if it send really, i don't know if the RX side that is faulty ...?
i don't have any spectrum analyzer to valide my TX side. only scope
i have search and search any tutorial. find some code but i'm not a C guru and work with BASIC language. so all is confuse, the codes samples are too much complicated.
i search the simplest tutorial to put a TX node and an RX node. to validate all the hardware / software side before do more stuff.
Please any CC1101 guru can help me ? point me on the simplest configuration ?
i try to use smartRF and don't find how create my own configuration. in the easy mode, there is 902, 868 and 433MHz. my module are tuned for 915MHz.
so i'm not sure about what i do :(
Please any help would be appreciate.. i turn around since 2 weeks !
Thanks for all suggestions, best regards
Phil