Other Parts Discussed in Thread: CC2511, CC2510
Hi,
Just to let you know, we have recently posted a question regarding CUDAL availability; the one presented in this post is more of a technical issue.
Basically, we have recently purchased a Development Kit for the CC2510/CC2511, coming with its 2 SmartRF04EB boards. We already had a Mini Dev Kit and bought the full Dev Kit out of interest for its extended features. Having acquired some programming experience with the Mini Dev Kit and IAR EW Kickstart v8.11 (the only version for which a kickstart license is currently offered), we tried programming chips from our SmartRF04Eb boards. SmartRFStudio and the Flash Programmer both recognize the CC2510 chip with both boards, but we only managed to program the chips with one of the boards. Basically, what happened can be summarized here :
With the first SmartRF04EB board, both IAR (with its .d51 files) and the Flash Programmer (with the precompiled hex files) couldn't program the chip, as the process always sent us errors with mentions ''Chip is locked'' or ''Flash erase failure''. We even tried both interface speeds with the Flash Programmer, and tried everything again after installing the latest firmware update (0045), to no avail.
With the second board, we managed to properly program both of the provided CC2510s (event without the board's firmware update). HOWEVER, we only tested the Flash Programmer's functionality on it, as we feared IAR (or maybe some wrong settings we gave to it) might have been the cause of Board 1's demise. Other explanations we can imagine for this board not working could be electrical problems or some fabrication defects. Of course, the question here is : what is this cause, and how could we solve the problem of Board 1's malfunction?
If you want, we can provide extended details on the different tests and attempts we did with the first malfunctioning board. These details are pretty long, however, so that's why we didn't include them in the current post.
Thank you in advance for your answers.