Other Parts Discussed in Thread: CC-DEBUGGER
Hey guys,
I am trying to use the CC debugger to program a few demo applications to the CC2540DK-MINI using the RF flash programmer and I am having some very frustrating issues that I'm hoping somebody can help me with.
I followed the instructions on the getting starting guide that was provided with the development kit. I first downloaded and installed the smart FT flash programmer and smart RF studio.( I read in the user manual for the CC debugger that the USB driver is automatically downloaded when any one of these tools are installed).
Now when I connect the CC Debugger to the PC I get an error from windows stating that the USB device not recognized. Specifically the error says that "One of the USB devices attached to this computer has malfunctioned". It says windows has stopped the device because it has detected problems( code 43).
I downloaded the Cebal – CCxxxx Development Tools USB Driver for Windows x86 and x64” which is a standalone installer including only the device driver and manually tried to update the drivers but it says that "the best drive for software is installed and up to date".
I tried connecting the debugger to the USB dongle and the keyfob and I know it connects to both targets because there's a green light on the debugger. So the debugger recognizes the targets but the PC doesn't recognize the debugger.
Has anybody faced this issue? I would really appreciate any help regarding this. I am using 64 bit windows 7.
regards,
V