I have interfaced CC1101 with PIC 24 micro controller . My task is to receive the signal from the door sensor . The sensor, which i bought from the local market and which is 433 MHz. I read the datasheet of CC1101 , where we i found ASk FSK type modulations used . So my question is that can i use this module with same modulations to receive signal from my door a sensor ?
Thanks in Advance.