Other Parts Discussed in Thread: CC1101
We are trying to read an RF signal from external Door sensor(433 mHz). I have used the application note of DN022 for configuring the cc1101 as ASK/OOK mode. We configured GDO0 PIN as data output pin. The CC11101 detect the sensor triggering , but the read bit pattern is always different. I was trying with different data rates on both the sensor and the CC1101 device, but the effect is same. The pin GDO0 by default is at logic level 1, but my sensor transmits start bit is also as Logic 1 , so we cannot identify the start bit correctly . This is also another problem.
So my questions are
1. Why the PIN GDO0 is always high after we configured the CC1101 in asynchronous mode? . Can we change the logic level of PIN by default ?
2. Why MCU always collect different bit pattern from the sensor ? Is it because of noise effect ?
3. Why the CC1101 detect some junk values with out sensor triggering?
I was trying to solve the issue for the last three days , but the result is not good.
Any help will be appreciated.