I have 42 new RI-RFM-007B-30 modules and 6 of them are failing at the same point. The failure seems to be at the 7805 DC regulator (IC101) which is heating up. The faulty modules are drawing around 60mA/5v instead of 20mA, like the working ones. I'm using the modules in combination with the RI-CTL-MB6B.
Any suggestions?
Thanks
Wayne