This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970A: Reset IRQ Status Register

Hello,

 

from the Datasheet:

"The status register is set to 0x00 at each write to the ISO control register. It is also automatically reset at the end of a read phase of the IRQ status register. The reset also removes the IRQ flag."

It is not 100% clear from the above sentence. Does a write to the ISO control register also remove the IRQ flag (IRQ line)?

Kind regards

Marco